|
Prefix |
Event Type |
Description |
|
BA |
BA Alarms |
A burglar alarm signal. |
|
HU |
HU Alarms/Panic/Duress |
A hold-up alarm signal. |
|
NPD |
Notify PD |
A signal to notify the police department. |
|
NPT |
Notify PT |
A signal to notify the patrol guard. |
|
FA |
FA Alarms |
A fire alarm signal. |
|
NFD |
Notify FD |
A signal to notify the fire department. |
|
MA |
MA Alarms |
A medical alarm signal. |
|
NMD |
Notify MD |
A signal to notify the EMS (Emergency Medical Services). |
|
OC |
Open/Close |
Open - a signal that the alarm is disarmed or turned off. Close - a signal that the alarm is armed or turned on. |
|
SU |
Supervisory |
A sensory device that monitors abnormal conditions, e.g. high temperature or water leaks. |
|
TR |
System Trouble |
A signal that indicates that there is a problem with the normal operation of a system. |
|
|
Actual Events |
BA, FA, HU or Medical signals is received by the Customer Monitoring Center that an actual event occurred from the customer/authorities. |
|
FO |
Fail to Open |
A burglar alarm signal is not disarmed when an Open alarm was scheduled. |
|
FC |
Fail to Close |
A burglar alarm signal is not armed when a Close alarm was scheduled. |
|
EO |
Early Open |
A burglar alarm signal is disarmed earlier than the Open scheduled time. |
|
EC |
Early Close |
A burglar alarm signal is armed earlier than the Close scheduled time. |
|
LO |
Late Open |
A burglar alarm signal is disarmed later than Open scheduled time. |
|
LC |
Late Close |
A burglar alarm signal is armed after the Close scheduled time. |
|
|
Bypass Zone |
A user enters a valid code for a zone to not trigger a fire alarm signal. |
|
|
Call Customer |
The Customer Monitoring Center contacts the premises or a person from the Contact list. The Dashboard Details will show the name of the contact and time of call. |
|
CA |
Cancel Alarm |
A user enters a valid code on the keypad after an alarm signal is activated. |
|
CC |
Critical Condition |
A special type of supervisory service used for monitoring critical areas (chemical leaks, blood banks, medical labs, etc.) |
|
CF |
Communications Failure |
Potential trouble with a phone line or communication device used by the alarm system. |
|
CL |
Close/Armed |
A burglar alarm signal is armed for an indicated location or area. |
|
CM |
Carbon Monoxide |
A signal indicating that Carbon monoxide is detected. |
|
DE |
Data Entry |
Internal events which display certain types of changes to the account information. |
|
FR |
Fail to Restore |
A device (heat detector, hold-up button, etc.) has failed to reset or restore as expected. |
|
FT |
Fail to Test |
An alarm system did not send a test signal to the Customer Monitoring Center as expected. |
|
GT |
Guard Tour |
A special service to monitor guards patrolling a location. |
|
IC/IF |
Supervised Communication Failure |
Potential trouble with the high security phone line or communication device used by the alarm system. |
|
IN |
Information Signal |
Information or status report. |
|
LB |
Low Battery |
A power problem typically caused by power outages or weak batteries. |
|
OA |
Operator Action |
Interval events which display actions taken by our operators. |
|
OP |
Open/Disarmed |
A burglar alarm signal is disarmed for the indicated location or area. |
|
RA |
Resume Alarm |
An internal reminder signal typically used to mark an account which requires follow-up. |
|
RE |
Restore/Rest |
An alarm device has returned to normal status after generating an alarm or trouble signal. |
|
SP |
Special Processing |
Special services or technology used by Johnson Controls. |
|
TA |
Tamper |
An alarm device that has been tampered with. |
|
TR |
Trouble |
Potential trouble with an alarm system or device. |
|
US |
Undefined Signal |
A signal type that is not defined in DataSource. |
|
UF |
UL Fire Alarm |
Underwriters Laboratory Listed System Fire Alarm. |
|
UL |
UL Burglar Alarm |
Underwriters Laboratory Listed System Burglar Alarm. |