The User Management section allows you to manage your user profile and contains detailed information that was initially setup in DataSource.
Users can update their personal information; however, administrators have access to adding, changing, copying, and deleting the user profiles.
To access the User Profile panel:

Note: From the Level Structure section, select the desired site levels to include in the report. You can search site levels using the Level Structure, Favorites, or the Search tab


Displays the site level that is selected from the Level Structure section.
Displays the current state the user is assigned in DataSource (Active or Inactive).
Active - By default, the Active setting is displayed in the Active field. Active users have access to DataSource, and their permissions are based on the account type that was set up by the Administrator.
Inactive - Users who have an inactive status are those whose permissions or access to DataSource has been disabled.